This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC39002均流设计

Other Parts Discussed in Thread: UCC39002

各位专家你们好,我最近在做一个均流控制,参考文档《UCC39002 Advanced Load-Share Controller User's Guide, HPA027A》进行设计。根据文档可确定大部分待定的阻值和容值,只是与CS+引脚连接的R7,R16,C1不知是如何确定的。在文档中关于这几个元件只找到这样一句话:The total impedance at CS− must be mirrored at the non-inverting input, CS+, of the differential amplifier, as shown by R7, R16, and C1 in Figure 1.

    谁能告诉我,这几个值是怎么确定的呢?还有一个问题:设计时,需要计算频率测量模块的单位增益交叉频率,这是一个什么参数?为什么要计算它?

  • 亲;电流信号输入采用的是差分形式。R6/16、C1是差分平衡RC,对应的值分别为R19/R22、C4。它们分别对应相等。

  • 差分放大,R7=R9,R16=R22,C1=C4,R16/R7为查分放大的倍数,这几个参数很好确定的。单位交叉增益的计算在技术规格书第几页?

  • 不好意思,是单位增益交叉频率,在规格书第7页的6.1.现在我知道这个量是波特图上0DB对应的频率,这个频率与RC补偿有关。不过关于UCC39002我还是有以下几个问题,还望您能指点一下:

    1、规格书的17页,有以下截图:

        里面说到a zero at approximately 1100 Hz, one pole at 10 kHz, and a double pole at approximately 200 Hz,请问这个频率分别是什么频率?怎样求得?

    2、在规格书21页有提到 POLE is equal to the added high frequency pole for noise roll off:
    POLE = 50 kHz

    其中的 f POLE是增益频率曲线的最高频率吗?

    3、在前面的设计方法中提到:

    在后面的实例中:

    请问 f ZERO在后面实例中除以100的依据是什么?

    问题有点多,英文水平也不怎么好,还望您能帮我一下