This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116输入电压和输出电压差的问题

Other Parts Discussed in Thread: LM5116

利用LM5116宽电压输入范围特性设计一个项目:要求输入范围18V~100V,输出电压范围15V~24V,测试过程中发现一个问题,在设定输出为15V的时候,降低输入电压到23V左右时,输出电压下降到不足5V;把输入电压调到24.5V左右时,输出电压回升到15V。。。。也就是说在输入电压高于24.5V时,输出电压可以在15V~24V间任意调节;在输入电压小于23V左右时,输出电压不能稳定在设定值15V左右。请问如何解决这个问题?

我只需要调整到最小输入电压18V时,能产生稳定的输出电压15V就达到要求了。。。。。