This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求解:LM5116输入电压低不能保持稳压输出



目前已经实现了在输入电压大于24.5V时,可调电压输出15V~24V。

但发现在输入电压低于22.5V时,不带负载的情况下输出电压减小为不到5V。带上200欧和100欧的负载,结果也都是一样。

项目要求输入电压18V时,能稳定输出15V就可以。

请TI的各位大侠帮忙解决这个问题,谢谢了。。。。