设定输出范围为13V~20V,实际调试中发现:
1>输入电压<24.5V时,LM5116不能正常启动,输出电压<5V;
2>设定输出电压13V,24.5V<输入电压<33.9V,带25欧负载,系统能正常稳定输出;输入电压>34.0V时,输出电压<5V;
3>设定输出电压20V,24.5V<输入电压<26.9V,带25欧负载,系统能正常稳定输出;输入电压>27.0V时,输出电压<5V;
请各位看看问题出在哪里?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
设定输出范围为13V~20V,实际调试中发现:
1>输入电压<24.5V时,LM5116不能正常启动,输出电压<5V;
2>设定输出电压13V,24.5V<输入电压<33.9V,带25欧负载,系统能正常稳定输出;输入电压>34.0V时,输出电压<5V;
3>设定输出电压20V,24.5V<输入电压<26.9V,带25欧负载,系统能正常稳定输出;输入电压>27.0V时,输出电压<5V;
请各位看看问题出在哪里?
继续报告测试进展:
更换电感测试,前面测量采用供应商送过来的1个样品电感,现在把3个电感样品并联,测试结果现象有改进,如下:
1>输入电压<24.5V时,LM5116不能正常启动,输出电压<5V;------本项性能无改进
2>设定输出电压13V,24.5V<输入电压<60V,带25欧负载,系统能正常稳定输出;输入电压60V以上暂未测试,已经满足实际项目需要,结果OK。
3>设定输出电压20V,24.5V<输入电压<30V,带25欧负载,系统能正常稳定输出;输入电压>30V时,输出电压<5V;-------该项指标有改进
测试进展之二:
在前面用3个电感并联的基础上,更改5脚(RAMP)到16脚(VCC)的上拉电阻,原为270K,更改为820K,测试结果有近一步改进,如下:
1>输入电压<24.5V时,LM5116不能正常启动,输出电压<5V;------本项性能无改进
2>设定输出电压13V,24.5V<输入电压<60V,带25欧负载,系统能正常稳定输出;输入电压60V以上暂未测试,已经满足实际项目需要,结果OK。
3>设定输出电压20V,24.5V<输入电压<33V,带25欧负载,系统能正常稳定输出;输入电压>33V时,输出电压<5V;-------该项指标有进一步改进,争取调整到40V左右