This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596输出-12V

Other Parts Discussed in Thread: LM2596, TPS5430, TPS54340, TPS54540

本想利用LM2596输出-12V,但是怎么也输出不了-12V,输出的只有-0.4V左右,不知道为什么。于是,上网搜了许多关于LM256输出-12V的资料,给出的解决方案基本都是调大电源的可输出电流。因此,我也调大电源的可输出电流到2.96A(这是我那个电源的最大可输出电流),但是输出仍是-0.4V左右。难道2.96A还是太小了吗?还是其它的原因吗?

下面是LM2596的原理图

                     

  • 亲;建议传一下你的相关PCB图。

  • 1.请问下你的电感的饱和电流是多少呢?

    2.启动的时候带了负载么?

    实在不行 可以尝试TPS5430 转负压,有成熟的验证过的电路。

  • Jason Shen 说:

    1.请问下你的电感的饱和电流是多少呢?

    2.启动的时候带了负载么?

    实在不行 可以尝试TPS5430 转负压,有成熟的验证过的电路。

    1.我使用的电感饱和电流是3A,启动的时候是空载的。试了好多次,输出电压就是零点几伏,有时也会是负的零点几伏,并且芯片和电感表面温度都很高。难道是电感的问题和没有带负载的问题?

    2.我看了一下TPS5430的资料,虽然能够输出-12V,但是输出电流好像只有0.5A,满足不了对后面负载驱动的要求。因为后面的负载是一个集成的开关电源模块,需要正电源和负电源的驱动,并且启动电流要求达到2.5A左右。

    3.我可能要换芯片了,LM2596实在搞不定。能帮忙推荐一款可以输出负电压(-12V)并且可以输出大电流(至少2.5A)的芯片吗?

  • 您好,TPS54340,TPS54540可以尝试下,耐压比较高,电流比较大。 TPS5430估计也是可以到2A左右的,注意散热。

  • Jason Shen 说:

    您好,TPS54340,TPS54540可以尝试下,耐压比较高,电流比较大。 TPS5430估计也是可以到2A左右的,注意散热。

    好的,我先试试。谢谢啦!

  • 恕我直言,空载无输出只能是电路有错的节奏。。。与原理无关。