This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116带负载烧掉原因

Other Parts Discussed in Thread: LM5116

项目基本功能实现后,带正常负载(带24V直流电机)工作,设定最大输出电压小于20V时,系统连续工作30分钟温升正常,系统输入功率在30W左右。

为了测试提高输出功率,设定最大输出电压为24V,输入电压61V,系统输入功率在40W左右,频繁启动、停止电机负载工作,不到100次,LM5116冒烟损坏,在19脚附近可以看到明显烧掉的痕迹。更换一个新的LM5116,系统又运行正常。

想问一下:这种情况下的LM5116烧坏是因为过热吗?如果是因为输出电压高从而输出功率也大,那我可以调低输出电压降低输出功率;如果不是因为输出功率过大,那么可能是什么原因呢?