This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在做无线充电应用。我按照BQ51013EVM-725 来做的板,元件参数也是参照 资料上的物料清单来焊接的。现在我测试得到的输出电压随输出电流的增加变化很大。空载时输出电压5.03V,但输出电流0.45A 时电压降到了4.9V,输出电流增加到0.8V时,输出电压才4.4V,而且输出电流不能达到1A,我用来设置电流的电阻是220欧姆。请帮我分析一下原因,以及需要怎样对策,谢谢!
Jinfeng,
注意看下RECT PIN的电容是否是20uF左右的,layout走线是否较短且铜箔较宽,量测下带载0.8A时,RECT PIN电压波形如何?若使用220ohm限流电阻,应当可以带载1.2A左右,强制带载1.2A,输出电压如何?会直接shutdown么?
Luke
RECT PIN 的电容我采用的是 4.7uF X 4 ,距离很短。我采用的是一个纯电阻负载,当我调整电阻,使输出电流增大时,电流在0.85A左右时就shutdown ,如果我在底下加一散热片,辅助散热,shutdown时输出电流就可以跑到 0.91A 左右。而且在工作的过程中,随温度的上升,电流会下降