用BQ24251充电,用的是TI的参考设计结合到自己的主板上,工作在SA模式下,但是在使用ISET和ILIM配置充电电流的时候无法成功,设置成多大充电电流都在700mA左右,和开发板对比ILIM管脚电压值为0,请问这是什么情况。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用BQ24251充电,用的是TI的参考设计结合到自己的主板上,工作在SA模式下,但是在使用ISET和ILIM配置充电电流的时候无法成功,设置成多大充电电流都在700mA左右,和开发板对比ILIM管脚电压值为0,请问这是什么情况。
你好,如果cc电流达不到,建议检查输入端adapter是否符合bc1.2 关于dcp的规格。谢谢!
你好,使用的充电器的CC电流在TI提供的开发板上最大能够达到1.5A以上的,但是在我自己做的板子上面只能达到700~800mA,这种情况下,ISET的管脚电压可以测得0.16~0.3V,但是ILIM的管脚电压一直是0V,两个管脚都是按照电流配置计算参数分别连接125Ω、135欧姆电阻接地,目前一直没有解决这个问题,请帮忙,谢谢!
再追问一个问题,使用SA模式时用外部电阻设置充电电流值,能达到最大的充电电流2A吗,IIC进行配置的时候一次配置完成下次重新上电后是芯片默认值还是上一次配置的值,谢谢!
问题已经解决,原因是芯片的D+/D-使用的时候用0欧姆电阻连接,在最初测试的时候把这两个电阻断开了,把断开的地方重新连接上问题就解决了。