现用BQ27541-V200做电池管理,电池容量4000mAH, 4.35V电芯,做golden sample时候发现通讯数据到4.18V就显示容量100%, FCC满充容量只有3800多,做完 Update Status也没变06,RaTable也没0055出现,求大神指教下可能是哪里有问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
然后充电时,请检查充电器的输出电压是否足够,确保不会因为输入源的线阻导致实际给到电池充电的电压不够。谢谢!
FCC容量不准问题,主要看你烧录的ID是不是和你电芯相匹配,只有匹配了,老化后更新出来的FCC值才是准确的。另外Update status没有为06,就代表没有更新成功。ID不匹配或老化不满足条件,都有可能造成更新不成功,你最好一一检查下各项条件你做得是否是对的。另外注意这个IC在老化前需要下21指令打开使能。