This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教个关于用干电池升压的问题

Other Parts Discussed in Thread: TLV61220, TPS61090

现在在做一个方案,用一节干电池(3V)升压至4.2V左右驱动一个网络模块。请问万能的TI,我选择贵司哪款升压IC比较合适,其中有几个值得注意的问题是:

1.当电池在使用后期,其电压会逐渐降低至2.5甚至更低。所以我期望其最低的升压电压能低至2V左右。

2.在产品正常工作的时候,其电流比较下,低于100mA.但在发送数据的瞬间,其电流可达到2A左右,所以我想其最大电流不能低于这个值。

我在网站上面看了TLV61220貌似还可以,不知道是否还有更合适的。

另外,以前这个产品是用FP6291,他的缺点是最低电压有点高。     

  • 1、TPS61090,或者你说的TLV61220最低工作电压都满足你的要求,你可以看看资料。

    2另外,你发送数据的时候持续时间有多少?频率是多少?有时候不一定需要那么大的额定电流,瞬时电流可以由输出电容提供。

  • 时间大概是600ns,现在我打板测试发现在电池电压2.8V以上是很正常,但在电压较低的时候会出现莫名的烧IC的情况,后面检查板子发现上面有个1000uF的电容(以前用来测试的)没有及时去掉。另外还有个330uF电容。请问其在低电压下被烧(拆下来量发现是SW脚对地短路)是因为此导致的吗。因为按照以前的经验,输出电容大点比较好。