Other Parts Discussed in Thread: TPS54560, LM5175
大侠们好,希望寻找一款满足输入10V~20V直流输入,输出也为直流,输出电压12V,输出电流最大为5A的DCDC转换芯片,用于电池供电,已看过TPS54560,不知道有没有用跟合适的,最好能手工焊的,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,这种应用可以使用LM5175。输入电压3.5V~42V,升降压控制器,需要外加MOSFET,非常适于动力电池供电系统。下面是芯片的链接,
http://www.ti.com/product/LM5175
可以直接使用webench去做仿真:
下面是用webench做的参考设计:
楼主,可以的,如楼下XP兄所说,注意散热,这个芯片底部是带散热焊盘的,底下铺地,再通过4~6个过孔连接到底层地,帮助散热 ,具体布局可以参考规格书第37页。