最近有个项目用TPS65140这颗芯片给LCD提供所需的各种电压,电路如下,现在板子上VREF、FB1电压正确,其余想要得到的电压都不正确,FB4输入电压应为3.3V,但是做的几块板子上只有一块为3.3V,其余都是4.2V,各位大侠有没有遇到过这类问题的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近有个项目用TPS65140这颗芯片给LCD提供所需的各种电压,电路如下,现在板子上VREF、FB1电压正确,其余想要得到的电压都不正确,FB4输入电压应为3.3V,但是做的几块板子上只有一块为3.3V,其余都是4.2V,各位大侠有没有遇到过这类问题的
楼主,先看一下你SW点的波形是怎样的,看一下AVDD电压是多少V,后面两路的VGH和VGL都是从AVDD引的电,另外看一下你电路中的二极管是否接对了方向,特别是BAT54,2个二极管在同一个里的,注意阴极阳极是否有问题,建议用万用表测试一下。
量过了,好的板子上SW输出的是方波,坏的板子上SW输出的是低电平,出现这个现象的可能原因有哪些呢?芯片坏了?
另外就是,手里有两块板子,能正常显示,但是FB4的输入电压都为4.2V左右,不是手册上写的3.3V,请问这可能是什么原因呢?NPN的三极管使用的也是手册上推荐的BCP68
量过了,VBE压差只有0.003V,输入输出电容都换成了4.7uF,FB4的输入电压还是4.0V