This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116用手焊焊机输出作为电源有问题。。。。

Other Parts Discussed in Thread: LM5116

用稳压电源作为LM5116输入电源时,从15V到62V都能正常工作,带动24V的直流电机;

但用直流输出的逆变焊机作为电源的时候,试焊焊条,焊条一点焊接工件还没起弧LM5116就烧坏了。焊条一点焊接工件,就相当于LM5116的输入电源在短路起弧,这个时候负载电机是工作的。还有一个情况,在焊条一点焊接工件是短路起弧,但是一般都是短路后会立刻和焊接工件断开的,断开后,是不是直流焊机输出电源回路串联的电抗器产生反电动势,从而电压很高击穿LM5116呢?因为我在LM5116的输入电源上接了一个1.5KW的91V的TVS管,在短路起弧的时候,TVS管都是立刻烧掉,连TVS管脚附近的铜皮都烧断了。

想问一下这是什么原因坏的?LM5116设置的ULVO管脚。输入电源小于14V就停止输出的。

如果是因为电抗器的反电动势电压很高击穿LM5116,这样该怎么处理啊?头疼。。。。。