This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
按照参数表,以13V为准。 但是实际不建议采用接近13V极限的电压。
如果你是15V输出,可以采用增加多个二极管或者便宜一点的LDO得到符合要求的Vcc电压即可。
Hi
是否采用外部供电VCC不是看负载,是看输入,如果输入电压比较大,例如35V,到LDO输出8V, 压差就是27V,芯片内部LDO的功耗就是27V*7mA=169mW, 按照40℃/W左右的热阻来算,大约会造成芯片7℃的温升。 所以如果输入电压更加的高(毕竟支持100V), 那么就就是采用外部电源。如果其实不是很高,例如举例的35V,其实造成7℃的温升,并不是特别高。
Hi
另外就是注意芯片PowerPad的散热设计,这个直接关系到芯片的热阻大小, 可以参考datasheet上面的要求,以及芯片底部可以打孔到背面增加GND散热面积等。