This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ3055一直处于INIT状态求助

Other Parts Discussed in Thread: BQ3055, BQ24133

RT,自己设计的BQ3055+BQ24133的板子,之前在Sheldon Cai的指导下成功让BQ3055唤醒并可以通过SMBus读取信息(这里表示感谢)。但是目前还是无法正常工作,INIT位一直为1,WAKE位为0.

具体表现为:

BQ3055的INIT, DSG状态位为1(BatteryStatus: 0x00C0)

BQ3055的寄存器显示两个FET没有开启(PF1, PF0 为1 0, ManufacturerStatus: 0x8000)。

CHG和DSG的FET一直处于关闭状态。

BQ24133也无法对PACK端充电(闪灯),PACK端无输出(100mV)。

OperationStatus: 0x8040,其余各种State都是0.

我想咨询下:

①为什么一直处于INIT状态?手册上不是说大约1s后就可以解除INIT状态了么?我该怎么进行下一步设置?

②我的电路没有设置二级保护,FUSE管脚悬空了,查了3060的资料,是否3055的FUSE引脚也必须接地?

附上原理图BQ3055与BQ24133(通过PACK端充电,电池电芯走123S,电池两端大电流走BAT±)

调了好久都过不去这个坎儿,万谢!!!!!