开发bq27200,直接读取芯片EEPOM中的信息,还是需要对EEPROM提前做一些初始化或是预置默写值或则芯片需要经历一个充放电周期(IIC协议编程都已验证好了)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
开发bq27200,直接读取芯片EEPOM中的信息,还是需要对EEPROM提前做一些初始化或是预置默写值或则芯片需要经历一个充放电周期(IIC协议编程都已验证好了)
需要根据项目的需求,修改相应的值。利用bq27X00 Battery Gas Gauge 这个Ti提供的开发软件可以进行开发。详见如下EVM使用手册www.ti.com/.../sluu210.pdf
完成基本的配置后,由于这个电量管理计是基于库仑计的技术设计的,所以需要一个full learning来知道实际的FCC等信息。
是不是必须在使用芯片签对芯片进行相关的配置,但是配置EEPROM需要21V的电压,还需要另外的设备支持,我是直接从你们那边申请了几块芯片,然后照datasheet上的典型电路,但是一直没办法读出数据,也没有对芯片进行配置,可否留下联系方式,咨询你?597174507@qq.com
请问我可以用EV2300直接读取一个已经有资料的BQ27200,然后再写进一个新的BQ27200里面去吗