您好:
在做12V电源冗余的时候遇到经过CSD17501的S端电压为12V,但D端却只有11.5V。
在进一步做试验发现
1.在没有焊接CSD17501的时候,TPS2412的BYP和GATE端的电压为22V,但是焊接了CSD17501以后BYP为22V,但是GATE却之后6.5V导致MOSFET 的Vgs = -5.5V,MOSFET的GS端为负电压,MOSFET肯定没有导通,请问为什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,TPS2412是通过VAC之间的电压来判断开通和判断MOSFET的,用NMOS是没有问题,不过对于走线比较严格。你测试一下芯片引脚A和C之间的电压,看看与MOSFET的S和D之间的电压,是否完全相同,有没有引入一些噪声。另,C引脚和VCC不要这样连接,C是直接连在MOSFET的D极,而VCC建议加个滤波,保证TPS2412的供电稳定。楼主可以看一下TPS2412规格书中的典型应用 电路和layout 指导。