请问要将两节锂电池输出的8.4VDC转换成12VDC用哪款芯片和电路,要求输出电压可调(通过反馈电阻),电流100多mA,用在仪表上,后一级是个射频电路?谢谢
注:输出电压不低于8.4V,电路越简单越好。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问要将两节锂电池输出的8.4VDC转换成12VDC用哪款芯片和电路,要求输出电压可调(通过反馈电阻),电流100多mA,用在仪表上,后一级是个射频电路?谢谢
注:输出电压不低于8.4V,电路越简单越好。
Hi
可以用TPS61170或者LM62014.
射频电路中对于电源要求很高,可以在其输出再增加一级LC滤波。
Hi
TI的射频DC/DC都是降压和升降压,并且电压输出都比较低,应该是没有可以做到12V的升压转化的.