This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询有关LED恒流驱动LM2791的使用问题

Other Parts Discussed in Thread: TPS62260

您好,我想咨询有关LED恒流驱动LM2791的使用问题

(1)LM2791的datasheet中提到,可以提供总共36mA的输出电流。由于LM2791有两路,如果两路都使用每路可以提供最大16mA。请问如果我只使用一路,最大输出电流可以达到30mA左右吗???我现在只需要用一路,并且希望这一路最大输出电流在30mA左右。

(2)LM2791主要针对白光LED驱动,我现在需要驱动一款LED Laser VLM-650-01-LPA (红色光,650nm),正向工作电压3~5V,工作电流<35mA,请问可以采用LM2791驱动吗???

谢谢,祝工作愉快!