最近在做PFC相关研究,调试了用UCC28070做控制器的PFC,有3个问题:
1,用UCC28070做的交错式3KW PFC的输出电压为380V,这个输出电压可以做成可调的吗,比如320~380V之间可调?
2,是不是用TMS320F281X(我想用这款DSP)将UCC28070替换作为主控制器,然后设计采集电感电流,整流后的电压,以及输出电压的采集电路,采集到信号后做一定的算法来达到功率因数校正的目的???
3,我想得到一个可变的电压,通过采用数字PFC方案,PFC的输出电压可以是变化的吗(比如320~380V之间可调)?当然电压会大于310V。