This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175输出过压保护和恒流应用

Other Parts Discussed in Thread: LM5175

LM5175的datasheet关于过压保护是这样描述的: ,我用了TI的一个参考方案“高效降压升压PWM-LED调光”,里面得恒流控制电路和过压保护电路如下:

方案说最大的输出能够达到35V。但我是这样理解的,D1阻断了电流流进放大器,也就是说电流只能从放大器流出,无论电流流向R1还是R2,都会使VF的电压增大。既然这样,我是这样理解的,当放大器输出电流为零时,只有Vo的增大使得VF增大,便可根据上述VF超过0.8V的7.5%便执行过压保护功能,计算出最大电压。VF=Vo*(R2+R3)/(R1+R2+R3),带入VF=0.86V,求得最大输出电压为4.3V。求大神看看是不是我哪里理解错了。


还有一个问题,参考设计是1.1A恒流输出。关于恒流,我是这样计算的:根据虚短虚断,VF=0.8V,设流过负载LED的电流为I,则 VFB=I*R5,又VFB/R3=(VF-VFB)/R2,算出来的I=0.887A。是我算错了还是因为电阻参数的分散性,R5是要调试的。求大神解释,拜托拜托啦