tps650245 输入电压为3.3V
输出
DC1 1.8V 1.6A
DC2 2.5V 1.6A
DC3 1.1V 0.8A
LDO 3V 0.2A
输入电压是否太低,是否有问题,这样做可以吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.