This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160启动问题

Other Parts Discussed in Thread: LM5160, LM25018

在测试LM5160芯片时遇到启动的问题,原理图如下

负载电阻+5V 250mA,-5V 50mA,按图中参数,FB管教正常工作时测到的纹波电压为100mV,启动电压为4.8V。但是有时候能启动,有时候不能启动。

去掉SS端的C13电容,启动变好,只是当输入电压以缓慢地速度加上去时,仍然不能启动,加快一点,则没有问题。

按芯片Datesheet,SS端要加至少1nF的电容才行,这和我实验测得的情况不一样啊。按理来说,FB端的纹波幅度大一点应该会好一点才是呢。

前面用过LM25018的芯片,也是同样的控制方式,只是没有LM5160芯片里面的GM放大器,也没有启动电容,但是LM25018启动很正常,无论多慢把电压加上去,都不存在问题。

希望能得到帮助,谢谢了!