This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74700-Q1: LM74700-Q1的驱动能力

Part Number: LM74700-Q1


如上,理想二极管驱动芯片LM74700-Q1的典型应用图,带负载的能力由外置的MOS决定,但是该MOS是否能驱动大电流呢?

比如说我选了个N-MOS:BUK7J1R0-40H,参数如下图所示。是否这个电路就可以带50A的负载呢?

按照正常的工作逻辑,LM74700-Q1工作时,是外部的体二极管先导通,然后MOS管才通道,那么MOS管导通稍微慢一点,是没有很大的影响的。

虽然LM74700-Q1对外置N-MOS的驱动能力很弱,但是这种应用不属于PWM型,属于开关型,就是上电的时候打开,下电的时候关断,不会频繁开关。那么N-MOS开通时间长一点,似乎没什么影响。

不知道我以上的理解对不对?

那为什么有的人说,用LM74700-Q1做驱动时,不适合带大电流的负载?

  • 就是说MOS是可以带50A负载,但是MOS带50A负载时,LM74700-Q1能否驱动MOS?

    LM74700-Q1的驱动能力是11mA,N-MOS的Qgd为17nc,那么开通时间=Q/i=17nc/11mA=1us

    按照这个算法,LM74700-Q1应该是可以驱动这个MOS的,不知道我的理解对不对?