This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54531: TPS54531

Part Number: TPS54531


1, 按TPS54531数据手册进行设计,用使能端进行输出控制,12V供电输入,使能端采用27K+13K,开关控制使能端是否接通12V,当12V供电后不接通使能时,是否可以认为使能状态下接到地了?

2 ,使能控制电阻 的选择与TPS54531的环路控制相关吗,不同的使能参数选取会不会影响环路性能?本电路使能的目的只是作开关用,无UVLO功能需求。

3, 空载条件下,现在的问题是完全冷启动时,输出正常为5.0V,但约30后输出变为0V。经检测发现是使能信号在启动后一直在变小,直至起不到使能功能。且该值并不为零,而是一直在0.3V~0.9V间变化(娄压表测量值 )。关机后短时间内再启动时,输出仍为零。只能是较长地间关机后,即完全冷启动才能出现上述的过程。

4 , TPS54531的输出滤波后,后级负载又需要做输出 滤波,再者在电路是距离很小,是否因两次滤波电容的并联造成原本计算设计的匹配电容量变化,导致输出不能稳定?