This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54360B-Q1: 电源管理论坛

Part Number: TPS54360B-Q1


用TPS54360B-Q1设计一个DCDC,输入电压范围:20VDC--48VDC,输出电压:28V,额定电流0.5A,峰值电流1.5A。

在输入电压低于设定的输出电压28V时,输出电压是否可以跟随输入电压呢?比如输入电压为24V,输出是否可以稳定在24V(稍微小一点)?

按照TPS54360B-Q1手册里的描述,应该是支持这种模式的,不知道我的理解对不对,麻烦TI的工程师帮忙看看,谢谢!