This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

遇到BQ24170的LED闪烁、VREF=3.9V情况时的建议

Other Parts Discussed in Thread: BQ24170, BQ24133

最近做了BQ24170的充电电路板,但遇到点问题,无法正常充电,表现为:
LED闪烁;
VREF=3.9V;

先确认了引脚AVCC、OVPSET、ACSET的电压,连接至引脚TS的电阻(103AT在25℃阻值约10k),这些都没问题;
之后拆掉了Q1、Q2,短接;
接上电池,LED仍然闪烁;

查阅了社区里关于BQ24170、BQ24133的帖子,基本上确认是焊接问题;

用万用表测量了相邻引脚的短接情况后,问题仍然没有解决;

后来没办法了,想想只有芯片背面PAD没有检查了;

于是,如同药商电视广告里讲的那样,我抱着试试看的态度,拿电烙铁在芯片背面补了几下,搞定了,VREF变成3.3V,充电时LED常亮,充满LED熄灭;

问题的根源出在PAD没有焊好,虚焊;

由此,总结出两点:

(1)BQ24170的PAD,正如数据手册第三页“PIN FUNCTIONS”表格所指出的,PIN NO.是THERMAL PAD,PIN NAME是AGND,不能单单认为是Figure 1中THERMAL PAD;
(2)画电路板时,正面PAD与背面GND/AGND的连接,最好有1个Hole Size为0.5mm的Pad(PAD指芯片,Pad指绘图软件),其余的可以用Via,Pad相对于Via的好处是,正面的锡刷多了更容易过锡,没有焊好的话更容易补焊;