This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: IIC通信在满足起始条件之后SCL和SDA始终被拉低

Part Number: BQ76952


使用NXP的MIMXRT1064作为主机,通过400kHz IIC与BQ76952进行通信,当IIC总线不连接BQ76952时,主机的IIC寻址命令可以正常发送,如图1(蓝色为SCL,黄色为SDA),但是当连接上BQ76952时,主机在发出起始信号后,SCL与SDA均始终被拉低,如图2(蓝色为SCL,黄色为SDA),无法进行正常通信。

BQ76952是照着数据手册画的原理图,IIC上拉电阻改成了1KΩ(如果是10KΩ会变成三角波),具体型号是BQ7695202PBFR,根据器件选择表,默认通信方式是IIC,CRC使能,REG1使能3.3V。使用万用表测量,REG1=3.3V正常,REG18=1.8V正常。

使用的电池组是10节18650锂离子电池组,电池组电压约为40V。

请问有哪些可能的原因导致SCL与SDA均始终被拉低?如何排查故障?

图1:

图2: