This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23754EVM-383: TPS23754 POE供电空载时MOS管发热严重

Part Number: TPS23754EVM-383

您好,

我这边设计POE模块,基本完全参考TPS23754EVM-383的原理图设计(差别:去掉的适配器供电部分,PPD悬空,APD接到AGND上),Rcls使用63.4欧即class4,VOUT输出为12.05V;

接上POE供电后,Q3和Q5区域慢慢开始发热,工作5分钟后,手摸上去有点点烫。

请问下TPS23754EVM-383的参考设计空载时本身就会发热严重吗?是否有相应有解决方案。谢谢!