This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118: 过流采样不准

Part Number: LM5118


LM5118 应用于buck `-boost 模式,输入电压为16-32V. 输出电压为26V. 输出过流保护电流为1A. 

在规格书中描述为在buck-boost状态下,使用0.255V/采样电阻=过流保护,但在实际测试中,实际保护电流比理论计算值要小一倍,比如设定为1A 的保护电流,却在0.5A 开始降低功率输出

1- 确认下为什么实际测试和理论值不一样?

2- 输入电压为16V ,输出为26V. 属于boost 模式,请问下这个阶段采样的计算公式是?

3- 输入电压为32V,输出为26V, 属于buck模式,请问你下这个阶段采样的计算公式是? 若两个计算公式不一样,那面对宽电压输入范围,该怎么选取合适的值?