This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: 关于RSOC在放电末端加速问题

Part Number: BQ40Z50-R2


hi,你好!

我在按下述步骤进行RSOC验证时发现2个问题,想了解该现象的原因和逻辑。

实验步骤:

  1. 常温下CC-CV模式将电池充满
  2. 将充满的电池放入恒温箱,设定恒温箱温度为0℃并开启恒温箱
  3. 开启恒温箱后静置2h
  4. 静置完成后进入恒功率60W放电
  5. 重复上述过程一次

问题1:

第一轮测试的结果显示RSOC精度整体均较差(>7%),重复第二轮测试后发现整体精度有改善,除去末端均<3%。请问此现象是否可以说明电量计在低温的性能需要经历一轮放电后才能提高RSOC精度?这块的逻辑是如何工作的?

问题2:

我在测试电量计低温放电的RSOC数据时发现其在10%左右会主动做加速,通过log数据回推得到的真实RSOC数据与上报的RSOC对比发现在RSOC>10%时的精度较高(<3%),主动加速后导致误差上升到8%。请问加速的原因是什么?如何解决加速带来的误差?