This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133和MAX17049应用时,BQ24133无法正常对电池插拔进行检测

Other Parts Discussed in Thread: BQ24133

应用BQ24133和MAX17049的原理图如下

     

VDC_IN=12V;VCC_IO=3.3V;

问题现象:将BQ24133的VBATT和MAX17049G+断开,VBATT处未接锂电池时,测量该点的电压为0.84V左右,接入电池该点的电压为8.4V,拔出电池VBATT的电压值回到0.84V左右;

将BQ24133的VBATT和MAX17049G+连接,VBATT处未接锂电池时,测量该点的电压为0.84V左右,接入电池该点的电压为8.4V(BQ24133的cell引脚是浮空的,两块电池),拔出电池VBATT的电压值一直保持8.4V左右;

将BQ24133的VBATT和MAX17049G+连接后,无法正常实现电池电量的检测,不清楚为啥拔出电池VBATT的电压值一直保持8.4V左右