1.TPS22996,当使能为低时,输出是对地短路吗?还是只是关断状态,输出为0伏?当使能为低时,TPS22996N的输出为“浮动”,浮动具体是何状态?
2.因为未找到低压(1.2V)的电源多路复用器或电源switch,我们想利用负载开关来实现双路电源复用器的功能,具体电路如下:
请问该电路是否可实现1.8V和1.2V的切换?如不能,该如何修改?或者有合适的IC推荐?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
TPS22996,当使能为低时,输出是对地短路吗?还是只是关断状态,输出为0伏?当使能为低时,TPS22996N的输出为“浮动”,浮动具体是何状态?
根据datasheet上的说明
如图所示当ON为L为VOUT=GND ,为H时VOUT=VIN 。TPS22996N为特殊情况会悬空。
请问该电路是否可实现1.8V和1.2V的切换?如不能,该如何修改?或者有合适的IC推荐?
根据的datasheet显示您的设计应该达不到。如果您不考虑驱动能力可以考虑电平转换IC。
这是多路电平转换IC,请您参考