你好,
TPS1H200A-Q1正常工作状态是12V800mA。
Delay引脚是选择接电容连接到GND模式,还是选择其他模式比较好?
您好
根据官方datasheet显示有两种模式您可以按照您的需求进行选择:
1、这种模式是您说的GND接电容接地的模式,是达到限电流保护模式,优势就是可以在突发情况下保护您的电路,缺点是保护后没有自动恢复。
Latch-off mode is active when the DELAY pin connects to GND through a capacitor. When a current limit is reached, the output current holds at the setting current, but latches off after a preset DELAY time (tdl1+ tdl2). tdl1 is the default delay time, and tdl2 is a configurable delay time set by a capacitor. Regardless of whether the current limit is removed or not, the output remains latched off. The output only recovers when IN is toggling
2.这种模式是接上拉的方式,达到限电流会保护后进行恢复。优点可以自动恢复,缺点如果不稳定的情况会导致IC处于不稳定状态影响工作稳态。
Auto-retry mode is active when the DELAY pin is externally pulled up. The pullup voltage must be higher than Vdl(th). When the current limit is reached, the output current holds at the setting current, but periodically turns on for thic(on) and turns off for thic(off). The device checks the current limit status at the falling edge of thic(on) clock. If current limit status is captured, the device shuts down for thic(off). If the current limit status is not captured because of the off window during the thermal conditions, the device keeps turning on for additional thic(on) or more until the current limit status is captured.
以上相关模式请您根据您实际情况来进行选择。