Other Parts Discussed in Thread: UCC28251
大家好,本人最近使用一款UCC28251的芯片,用于全桥控制,输入270V,输出28V/40A.在调试时遇到以下问题想请大家帮忙。
芯片外围电路与规格书中典型应用一样,测试时遇到下面几个问题:
1.设计的DC输入最低是220V,但220V输入时输出软启以下然后驱动关闭,无输出。为什么软启一下,然后就不发驱动了;
2.将输入电压调制120V,输出只有10V,然后把输入降低到80V,接着输入电压增加到120V,输出为28V变为正常,这个应该影响了RAMP/cs电压,但为什么会这样的现象。
3.芯片有时候回出现此现象,无驱动输出,SS,COMP脚电压为0。但此时芯片vref为3.3V,OVP为0,EN为2.8V。为什么芯片会停止工作?
谢谢