This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL494: 关于TL494输出PWM频率可调不稳的问题

Part Number: TL494


本人负责的产品为控制器,外部连接不同类型的配套负载。目前负载中放置一个不同阻值的下拉电阻,控制器通过电阻分压的的方式实现负载型号的识别。但是对3.3V进行分压,但受限于的电压范围及误差精度,按照0.1V一档才30种,很难做到扩充种类.

因此打算使用TL494搭建外围电路,通过外接的阻容,匹配不同的RC值(外接电阻R和板端的C805),使得TL494晶振频率不同,输出的PWM的频率也就不同(TL494的8管脚),这样可以无限扩充种类。但是测试后发现两个问题:(1)手册上写  f=1/RC ,但是实测理论100khz,实际才10khz;(2)输出的频率不稳定,每次都有一定范围的跳变,通过使用示波器观察,比如10KHZ会在9.3KHZ~10.5KHZ变化,因此很难通过MCU识别频率的方式进行型号区分,或者这个频率的误差范围就得设计的足够大,但是这就造成相应的种类就会少很多。

附件为电路图,请各位大神帮忙,看看是哪里设计的不对造成的??????????????求助求助求助