This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92641: 电流不按设计输出

Part Number: TPS92641


上面这样的一个原理图,不接PWM输入,接上LED之后输出电流就是20A,正常情况是PWM输出给100%的PWM波电流才会到达20A。

自举电容两端的压降是3.5V,靠近芯片boost端的电压是12V,自举电容处的二极管D3两端的压降是4V且boost脚电压比VCC电压高

不接LED灯的时候LED+与LED-的电压差是7.8V

请问一下,上述情况可能是原因是什么?