TPS25947: For switch design related problems

Part Number: TPS25947
Other Parts Discussed in Thread: PCA9535

Dear TI:

I want to design a power switch circuit with TPS259470,But Some Question:

1.My Circuit Designe 

EN/UVLO Connect to PCA9535, GPIO Level  is 5V,TPS259470 is controlled by I2C bus;When GPIO =H,TPS259470=ON,GPIO = L TPS259470=OFF;

OVLO Connect to GND;Close Overvoltage Clamp

2.Since my GPIO input is 5V, the input voltage of TPS259470 changes from 3-18V, and the EN/UVLO voltage is higher than the input voltage of TPS259470, is there any problem in this design?

3.OVLO is connected to GND to close the Overvoltage Clamp. Is there any problem with this design?

I would like to ask TI engineers to help answer the above questions!Thanks