This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5030: 推挽实现±15V输出,CS通过MOS到地的检流电阻进行电流限制,却无法过流保护的问题。

Part Number: LM5030


实际原理图如下,限流电阻取值修改为100mΩ。CS的RC取值750Ω和1nF。+15V输出短路,只达到0.5V的限流,输出保持了3A多的电流,并没有进入0.625V的重启式限流。请问这是什么原因?