This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51561: 请问该芯片的UVLO引脚受温度的影响吗

Part Number: LM51561

  如图所示,在A点设计了一个开关电路通过控制A点的开通关断,继而控制电源芯片UVLO引脚的电压,使得电源芯片能够开关机,现在的问题是,室温下测得一切都是正常的,芯片能够正常的开关机,在温度为50℃的时候,输入电压为12V时,发现下不了电了,A点关闭之后测量A点会有个5V左右的电压,此电压推测为ULVO脚内部电流源流经R334电阻所形成的电压,通过改变R310与R334电阻阻值,都为5.1K之后,温度为50℃的时候,能够实现上下电了,当温度提升至80℃的时候,测量发现又下不了电了。请问该现象是否为芯片内部设计问题还有有什么解决方法。