你好,我想了解下UCC28730的待机功耗,在SLUA968中显示UCC28730的待机功耗在220Vac输入下,输出5V/2A可以做到3.2mW,我现在要设计一款(300-1000)Vdc输入的车载电源,其中内部的辅助电源输出15V/1A,我想用UCC28730来做这个辅助源,请问UCC28730在(300-1000)Vdc输入下的空载待机功耗可以做到多少,能做到40mW以内吗?如果不可以有什么其他方案可以推荐吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
这是官方提供的计算器,您提供相关参数,它会给您相关功耗的评估

这是计算器的部分截图,请您参考。