This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54531: 使用TPS54531DDAR芯片电源输出有些问题

Part Number: TPS54531


使用TPS54531DDAR芯片,

 空载时的输出是6.5V;

当负载大于100mA时,输出开始下降,200mA时,电压会稳定在3V左右

使用datasheet手册的方案更改COMP端口连接电路,4块电路板只有1块能输出正常电压。

请问这个是怎么回事?如何解决呢?

谢谢!