This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: About internal temperature measurement

Part Number: BQ76952


Hi, the datasheet 7.22 Internal Temperature Sensor describes the ΔVBE measurement, how do I get the voltage value of the measured ΔVBE, and is there a register that records this value. Because I want to verify if this voltage value divided by 0.410 is equal to the temperature value.

  • 您好

    https://www.ti.com/lit/ug/sluuby2b/sluuby2b.pdf?ts=1721192350714

    基于官方TRM文件,关于这个部分有相关说明

    The BQ76952 device integrates the capability to measure its internal die temperature by digitizing an internal transistor base-emitter voltage. This voltage is measured periodically as part of the measurement loop and is processed to provide a temperature value using the 0x68 Int Temperature() command. This internal temperature measurement can be used for cell temperature protections and logic that uses minimum, maximum, or average cell temperature by setting the Settings:Configuration:DA Configuration[TINT_EN] configuration bit and keeping the Settings:Configuration:DA Configuration[TINT_FETT] bit cleared. The internal temperature measurement can instead be used for FET temperature by setting both Settings:Configuration:DA Configuration[TINT_EN] and Settings:Configuration:DA Configuration[TINT_FETT], although in this case it will not be used for cell temperature. The calculation of temperature is performed as follows: Internal Temperature (in units of 0.1 K) = (ADC value) × Calibration:Internal Temp Model:Int Gain / 65536 + Calibration:Internal Temp Model:Int base offset + Calibration:Temperature:Internal Temp Offset except if (ADC value) > Calibration:Internal Temp Model:Int Maximum AD, then the reported internal temperature is calculated using the Calibration:Internal Temp Model:Int Maximum AD as the ADC value. If internal temperature is calculated > Calibration:Internal Temp Model:Int Maximum Temp, the reported internal temperature is set to Calibration:Internal Temp Model:Int Maximum Temp.

    具体详细说明请参考上述连接。