使用TSP613222A 输出5V/500mA,采用4.2V 输入,未接负载测量静态功耗45uA,远远大于手册6.5uA,请问哪里有问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
1)什么测试方法?
静态电流的概念以及测试方法(见2)),您可以看一下下方关于IQ的概念,不仅仅是No load,也要nonswitching。具体见下方链接

https://www.ti.com/lit/an/slyt412/slyt412.pdf
2)1.2*target是什么意思?
TI没有公开测试方法,但是在之前给您发的帖子里面也有提到,将Vout保持在高于芯片的target value,是为了让转换器不进行switch,也就是1)中所说的nonswitching。您的这款芯片是固定输出的,那个值应该就是target。
3)我这个45uA属于正常的?
这个不是正常与否的问题,因为您只是no load,而不是no load&no switch,而且您外围也有很多电容电感这些容易产生小电流的器件,芯片的静态电流应该是芯片自身的。
您如果把您测的这个45uA当作是静态电流值,认为芯片不符合手册的6uA,这个是不合理的,因为您测的不是静态电流。