This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25830A-Q1: TPS25830A-Q1配置为CDP模式,连接手机无法充电

Part Number: TPS25830A-Q1


芯片配置:配置TPS25830A-Q1为CDP模式,CTRL1设置为1,CTRL2设置为1;频率设置:400K;电流ILOMIT:3.3A;USB对外接口使用type-c接口设计,正常连接CC1,CC2。

故障现象:连接手机后,手机不显示充电状态;测量VBUS发现电压为0.9V左右.

测量信号:EN正常为1;CC1/CC2正常拉低;Dx_OUT<2.2V正常;VBUS输出0.9V左右,异常;LD_DET为高,异常。

请问为什么出现这种现象。怎么避免VBUS无法拉低的情况。