This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: 是否可以应用于16-80Vin下的四开关拓扑?

Part Number: LM5176

您好,我有一个16-80V输入转28V的应用需求(无隔离要求),考虑体积与高效率,功率大概300W,想使用四开关Buck-Boost拓扑:看LM5176芯片工作电压范围为4.2V-55V,想请教是否可以通过以下改动,应用于16-80V输入的工况下,谢谢!

1)将SW1与SW2接地,使HDRV两路驱动参考地为公共地,另外加两组100V以上的高低边驱动器实现上管驱动;

2)芯片的VIN脚单独供电,输入电压Vin经过分压后送入芯片的VISNS,也能表征输入电压的变化;

或者,有没有其他的芯片或者方案推荐,谢谢