This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27441 使用问题

Other Parts Discussed in Thread: BQ27441-G1

各位好,最近在使用bq27441这款芯片检测电量。在使用中有以下几个问题想询问下:

1. 根据Quickstart Guide for bq27441-G1 设置好四个主要的属性值,给电池充电,soc到100%,管理电池充电的芯片用的是24295,充满电后流经27441的电流为0,经过1个多小时FC都没有置位,据说是阻抗表不匹配,不知是否如此。

2.充满电后,拔掉外接电源,用电池供电,几分钟左右后,soc会从100%突然变为28%。现象是由于使用外接电源时,电池电压为4.2V左右,使用电池供电时,电池电压会被拉低。但是库仑计的设计原理应该不只是靠电压检测电量的啊。难道也是阻抗表不匹配的问题?

3.如果阻抗表不匹配,那么是需要怎么让其匹配呢?只是进行一下电池的充放电就可以吗?

4.只用I2C的话,可不可以实现量产步骤,通过I2C就设置好匹配表?

在此先行感谢回复!

  • 是的,阻抗不匹配会导致电量计内部算法计算不准确。

    阻抗匹配需要充放电learning cycle,详见下面的精华帖链接。

    http://www.deyisupport.com/question_answer/analog/battery_management/f/35/t/46539.aspx

    learning cycle需要EV2300/2400工具,然后生成dffs/bqfs文件(都是I2C指令,里面已包含阻抗表),可以解析转换成I2C指令下载到MCU,进行量产。