AC-DC变换 24VRMS to 36VDC,输入先用直流输入调试时稳态Vout为36,Vsense可以达到5V,但是负载调到30欧左右电压开始急剧下滑,最低到28V左右。交流调试时Vsense始终没有达到5V,24V输入时只有32多V,Vsense只有4.7左右,而且随着网压、负载的变化,输出电压变化较大,最低到24V。不知道正确的分析顺序是怎么样的,希望技术人员及发烧友给予指导,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AC-DC变换 24VRMS to 36VDC,输入先用直流输入调试时稳态Vout为36,Vsense可以达到5V,但是负载调到30欧左右电压开始急剧下滑,最低到28V左右。交流调试时Vsense始终没有达到5V,24V输入时只有32多V,Vsense只有4.7左右,而且随着网压、负载的变化,输出电压变化较大,最低到24V。不知道正确的分析顺序是怎么样的,希望技术人员及发烧友给予指导,谢谢!
原理图我现在不在这台电脑
用IRF540作开关管
电感1.3mH使用ER42/45磁芯150匝 气隙增大到5mm 应该基本确保10A电感峰值电流不饱和(这里我想问 如果电感饱和会导致什么具体的问题可以分享一下吗?)
二极管使用SR3100(3A 是不是不太够?这只二极管是临时得到的)
电流采样电阻0.05欧(贴片 稳定性在一次过流之后可能不太好)
其他:其他参数Cout实际为8000uF左右
我想问28019周围的补偿元件作用是什么 是否起决定性作用?