各位专家好,我在将BQ76952用作8串电池管理时,通过电流表观测到top Cell的电流有1mA,然后通过检测图中R226上的压降确认电流确实有1mA。76952在我的应用中仅作为电池电压和温度采样,未生成REG1和REG2,同时也不参与充放电MOS的控制,不明白此处为什么有这么大的功耗存在?硬件是上是否功耗大的地方或者软件的配置会造成功耗大,请专家帮忙指导解答。
另外,下图中CH1通道(黄色)波形是我检测TS1端口的波形,当脉冲非常密集时应该是处于normal模式,当脉冲非常稀疏时是否进入了Deepsleep模式?这个问题的起因是我没有开启REG1和REG2,不知道通过什么标志来确认76952是否进入了Deepsleep模式,所以想用TS1的状态来判断。
Best Regards