This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS27S100: 如何实现可以限流6A

Part Number: TPS27S100


您好!

我们使用贵公司的TPS27100的芯片,输出接负载测试带负载能力,ILIM对地连接的情况下,工作环境温度25摄氏度,负载在3.7A的时候,这个芯片有保护关断再打开的现象,持续切换。

规格书上电流限制6A,请教一下如何实现可以达到6A的带载能力。

如果您方便可以打我的电话。

电话:15256015828